Product FAQs

Ask a Question

What is the BOM for 33247 ?

 The BOM for 33247 is the following :-
33058 MG LABEL
33071 MICROLOGIC 2.0 A
33093 1000A SENSOR PLUG
33100 INTERNAL TERMINAL BLOCK FOR CO
33121 SET OF NUTS FOR CONNECT 4P NS630B-1600
33133 1 FRONT CONN. TERMINAL SHIELD
33140 CHC MB SCREW L=16 WITH WASHER
33141 CZS D4 SCREW FOR CONN.TERMINAL
33148 OWNER MANUAL FOR NS 630/1600
33158 FRONT ESCURCHEON FOR COMPACT
33206  cb ns630b/1000 n manual 4
33416 perfomer n0 26 40 ka 40 
33542 STANDARD RATING PLUG 0.4 TO 1
34380 1 FRONT CONNECTION TERMINAL FOR NS630B/1
47579 1 LABEL ROLLER (2000)
64047 ns 1000 perf n name plate
Was this helpful?
What can we do to improve the information ?