Product FAQs

Ask a Question

What is the BOM for 33253 ?

 The BOM for 33253 is the following :-
64048 ns 1250 perf n name plate 
33416 perfomer n0 26 40 ka 40 
33158 FRONT ESCURCHEON FOR COMPACT
33542 STANDARD RATING PLUG 0.4 TO 1
33100 INTERNAL TERMINAL BLOCK FOR CO
33071 MICROLOGIC 2.0 A
34380 1 FRONT CONNECTION TERMINAL FOR NS630B/1
33094 1250A SENSOR PLUG
47579 1 LABEL ROLLER (2000)
33148 OWNER MANUAL FOR NS 630/1600
33058 MG LABEL
33001 NS630B/1600N/H MANU. OPERATED
33132 1 SET OF NUTS AND BOLTS FOR FR
33141 CZS D4 SCREW FOR CONN.TERMINAL
33140 CHC MB SCREW L=16 WITH WASHER
33131 1 FRONT CONN. TERMINAL SHIELD
33080 ENGLISH USER MANUAL FOR
Was this helpful?
What can we do to improve the information ?