Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Can M340 PLC be used BMXCRA31210 ?
The CRA Module can't be used with M340.
If you want to use CPU in the local rack and CRA module in the remote rack then you will need to use M580 PLC not M340.
If you want to use CPU in the local rack and CRA module in the remote rack then you will need to use M580 PLC not M340.
Did this answer your question?
Explore more
Explore more