{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Can I use the manual control actions in Diagrams in PME?

Starting from PME2020, You can use the manual control from the Diagram.
You can enable or disable the ability to perform manual control actions in Diagrams. 
Example: resetting values on devices or changing device configuration settings. Set the confirmation method that is used by the software.
Also, user can select the confirmation method - Dialog Box without Password or Dialog Box with Password.

Control in Diagrams is only available when a HTTPS connection is used between the PME server and the Web Applications client.
The required user access permissions for performing a control action are configured individually for each control object in a diagram. This is done at design time in Vista. However, to perform any control action in Diagrams you need at least controller-level access or higher (operator-level, supervisor-level)