Browse FAQs

Is it possible to translate alarm message history to another file format in SFT2841 software?

Published date: 13 September 2020

Issue :
Possibility to translate alarm message history to another file format in SFT2841 software

Environment/Product line:
SEPAM 20 40 60 80 relays

Resolution:
The STF2841 software is a setup and operating tool for Sepam series 20, 40 and 80 relays. It can be used in one of the following modes: 
1) Offline mode : Authorized for commissioning and without connection to Sepam relay to prepare protection and parameter settings
2) Online mode : During commissioning with PC and Sepam front panel connected via CCA783 series cable: download, transfer data and edit Sepam relay protection and parameter settings and
obtain all measurement and useful data during commissioning
3) Network mode : During operation, when the PC is connected to a series of Sepam relays E-LAN multipoint communication in the network to manage the security system,
monitor the status of the power network and perform diagnostics of changes in the network.

Final conulsion is SFT2841 software cannot translate history alarm messages into another file format for future use or storage.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.