Product FAQs

Ask a Question

Are the Altivar ATV18 fault contacts dry?

Issue:
Are the Altivar ATV18 fault contacts dry?
 
Product Line:
ATV18
 
Environment:
All
 
Cause:
N/A
 
Resolution: 
Yes, you can supply up to 250 volts AC at .5 amp.


 
Was this helpful?
What can we do to improve the information ?