How can we help you today?

I have a TSX Micro module, the " Ter " & the " Run " Leds are blinking and the I/O led is off ?

This means that the PLC is in the STOP mode. It has to be run using the program ( Connect the module to the PC ).

Schneider Electric United Arab Emirates