Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
Video: How is the Altistart ATS22 set for 3 wire control?
Issue:
Programming and wiring needed for ATS22 3-wire control.

Product Line:
Altistart 22

Environment:
All

Cause:
Installation

Resolution:
Wiring:
Wire a momentary normally-closed STOP contact to LI1 and a momentary normally-open START contact to LI2.

Programming:
Set LAC= On
In the I-O menu, set LI2 to Start (3 wire control).

Schneider Electric United Arab Emirates