How can we help you today?

I have " NST " error code on the ATV312 display and it doesn't want to run.

" NST " stands for freewheel stop mode.This means that the stop signal into one of the assigned logic inputs is cut ( since the freewheel stop function is active at " 0 " ).  So, you have to check the wiring.

Schneider Electric United Arab Emirates