What is the maximum breaking capacity for MCB Acti 9 of type iC60H according to IEC 60898-1 ?
The maximum breaking capacity for iC60H according to IEC60898-1 is 10000 A (10 KA)
Refer to the attached data sheet for iC60H MCB
Refer to the attached data sheet for iC60H MCB