Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
How to test ATV71 on low power motor or without a motor ?

Issue:
How can ATV61 or ATV71 drive run without the motor been connected to it?

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Needs to test the drive to see if there is a problem with the drive by running the drive open circuit, without the motor connected to it.

Resolution:
Under Drives menu, go to menu 1.8 Fault management.
Find Output Phase Loss, and set to NO

Then go to menu 1.4 Motor Control
Find Motor Control Type, and set to V/F 2pts if it is set to something different.

Note: Make sure to set Output Phase Loss back to yes after testing is done.   Some applications may also require the Motor Control Type to be reset to the previous setting.   Wear necessary protective equipment while testing with OPL set to off, voltage and current will be available at the output terminals of drive

Schneider Electric United Arab Emirates