Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
How can i update the M340 firmware?

First you need to download the required firmware version then do the below steps attached in the document
https://www.se.com/ww/library/SCHNEIDER_ELECTRIC/SE_LOCAL/APS/203659_0286/M340_upgrade_procedure.pdf

please check the below video :
https://www.youtube.com/watch?v=4ctaPNPtcKU

Here are the steps in brief
- Double click on the “patcher.bat” file
- In a command prompt window, the following text is displayed: NOE IP address?
- Type the IP address of the NOE:  e.g. 138.157.9.53 and then Enter
- Then appears the following message: Connecting to 138.157.9.53…
- If connection is possible then it displays the following message (checking if the NOE needs to be patched):  Checking...
- If the patch is not needed then it displays the following message and finishes the process:
Patch not needed!
- Otherwise it displays the following message and finishes the process by patching the NOE:
Patch is done!

Important notes

• After the Patch is done and before resetting the NOE, launch the UnityLoader and connect it to the NOE: the NOE can be upgraded.

• The Patch is only a temporary one (RAM): if you reset the module before upgrading it, the Patch is lost, and the module gets back to initial state before patching.

• Do not power off during the Patch and before upgrading it.

Schneider Electric United Arab Emirates

Attachment(s)
Modicon M340 Firmware - Update procedure.pdf [1.19 MB]