Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
does we have Steel enclosure with sheet thickness 2mm ?
We don't have in our offer the mentioned dimensions with thickness of sheet metal = 2 mm. Yet the IK, degree of protection =IK10 conforming to IEC 62262 (impact energy 20 J (40 cm , 5KG)).
So this guarantee the mechanical withstanding and we don't have any needs to have thickness = 2mm.

Schneider Electric United Arab Emirates