Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
We forgot the password of the soft starter ATS48 how can we reset it?
The master password for ATS48 soft starter is 999, you can enter the password menu. After this code will automatically return to 0.

For your information, there is a dip switch behind the REMOTE keypad, in position LOCK only the SUP menu is also available (please refer the installation manual for more details)

Schneider Electric United Arab Emirates

Attachment(s)
ATS48 Password.pdf [54.56 KB]