Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
What are the replacement SCR firing boards for the ATS48 soft starters?
Issue:
Replacement SCR firing boards for the ATS48 soft starters

Product Line:
Altistart 48  ATS48

Environment:
ATS48C41Y – ATS48M12Y models

Cause:
Replacement

Resolution:
The replacement SCR firing board is selected based on the ATS48 part number.
There are multiple boards per ATS48.
See the attached file.

Schneider Electric United Arab Emirates

Attachment(s)
ATS48 Firing board.pdf [124.07 KB]