Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
What is the sheet metal thickness for Prisma iPM System M?
For Prisma iPM system M, the sheet metal thicknesses are as follows:
  • Framework --> 2 mm
  • Rear panels --> - 1.5mm
  • Side panels --> 1 mm
  • Roof --> 2 mm
  • Bottom panels --> 1.5 mm
  • Front plates --> 1 mm
  • Door --> 1.5 mm

Schneider Electric United Arab Emirates