Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
what is the difference between Standard Data-Set and Legacy Data-Set ,in Modbus Communication NS,NT/NW ?
The standard data-set: is a global entity that collects the most useful information of each IMU module in one convenient table.
  • The benefit is that in one location there is up-to-date information with three read requests.
  • The standard data-set can be used with IFMv2 ,IFE or EIFE interface
  • The main information needed for remote supervision of a Compact NSX, Compact NS, Masterpact NT/NW or Masterpact MTZ circuit breaker is contained in the table of common registers starting at register 32000
  • The standard data-set is defined in the 32000 to 32435 register range.

The legacy data-set: is a global entity that collects the most useful information of each IMU module in one convenient table.
  • The benefit is that in one location there is up-to-date information with two read requests.
  • The legacy data-set can be used with IFM and IFE interface.
  • The main information needed for remote supervision of a Compact NSX, Compact NS, or Masterpact NT/NW circuit breaker is contained in the table of common registers starting at register 12000.
  • The legacy data-set is defined in the 12000 to12165 register range.
NOTE: The legacy data-set is compatible with previous versions of the Micrologic trip unit.

Schneider Electric United Arab Emirates