Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
How do I select the proper rated output (burden) value of my voltage transformer?

Sometimes one can select a relatively high value of rated output (burden) for a given voltage transformer as it is commonly thought the better choice when we are not sure about the typical burdens (loads) connected to our voltage transformer secondary.

IEC 61869-3 gives the standard values for rated output (burden) for a given voltage transformer:

image 1

image 2


In many cases where devices connected are mainly of micro-processor based protection /metering equipment, the overall burden can only be a few VAs; in other words a burden range (I) voltage transformer is considered adequate in many cases.

It is important to know that using an "oversized" voltage transformer rated output (burden) has a negative impact on accuracy thus increasing the error of the measurements.
The below highlights provides the limits of error which IEC 61869-3 specifies for each burden range.
image 3
image 4


Finally, it is important not to oversize your voltage transformer too far beyond the actual need for rated output in order to avoid increase of errors at a lower value of burden applied.

Schneider Electric United Arab Emirates