{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
How to achieve earth leakage protection in TT earthing system
According standard IEC 60364 4-41, for TT earthing system the protection must be ensured by RCD, the sensitivity Idn of which complies with the condition Idn<=50V/RA. In TT system, the fault current is limited by earth resistance and is generally well below the setting thresholds of SCPDs and ground fault protection threshold of micrologic 6.
SGR or residual ground fault protection is not convenient as the threshold are high than those recommended in TT.
Below a table giving choice about GFP and RCD relating the level of earth fault value.
Vigirex + toroid for TT earthing system solution would have been a good solution for the rating up to 3200A.
table.png

Schneider Electric United Arab Emirates

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.