Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
What are temperature settings required for "T" type thermal protection on Trihal dry type transformers?
The transformer rating plate shows temperature rise class "F", which requires the user to apply setting of the T digital thermometer/controller with a maximum temperatures of:
  • 140°C for "alarm 1" and,
  • 150°C for "alarm 2".

Schneider Electric United Arab Emirates

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: