Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
what is difference between ics and icu ?

1. Standard IEC/EN60898-1 specifies that a circuit-breaker having a given rated short-circuit capacity Icn has a corresponding service short-circuit capacity (Ics) according to table 18 - see Attachment1.

For example, the iC60N has Icn 6000A according to the standard IEC/EN60898-1 so Ics = 6000A;
the iC60H has Icn 10000A so Ics = 7500A,…

Schneider Electric United Arab Emirates

Attachment(s)
Attachment1-18731622.jpg [41.62 KB]