Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
Where can I download SoMove and DTM files? What is the USB to RJ45 cable required to connect SoMove to the drive using the ModBus port?
Issue:
Where can I find a link for SoMove?
What cable is used?

Product line:
Variable Frequency Drives and Soft Starts

Environment:
All models, all serial numbers

Cause:
None

Resolution:
Below are the Links for SoMove Software and DTMs for AC Drives and Softstarts.

(Somove 2.6)
https://www.se.com/us/en/download/document/SoMove_FDT/

(Altivar DTM files for the ATV61, ATV71, ATV12, ATV212, ATV312, ATV32)
(Altivar Process 600 DTM files)
https://www.se.com/ww/en/download/document/ATV6xx_DTM_Library_EN/

(Altivar Process 990 DTM files)
https://www.se.com/us/en/download/document/ATV9xx_DTM_Library_EN/

(Altistart DTM files for ATS22 and ATS48)
https://www.se.com/ww/en/download/document/Altistart_DTM_Library/

All other:
https://www.se.com/us/en/download/

Click on Optional Filters
Select Document Type Group: software
Select a Product Category - AC Drives and Softstarts
Select a Product Sub-Category - Process Drives
Select Product Range -
-  Altivar 61 (i.e. for all Altivar AC Drives DTM)
-  Altistart 48 (i.e. for Altistart Softstarts DTM)
-  Process
-  etc.
Click the Search button

Download the DTM files for altivar drives and the stand alone file for Somove.

WinZip or 7-Zip Extraction software may be needed for compressed/zipped files.  If needed you can Download Free version 7-Zip from; http://www.7-zip.org/

Below are the links from our FTP Site to the latest drivers for the TCSMCNAM3M002P cable.  The software is free online, however, you will need to purchase this cable to connect your PC to products via the resident Modbus port.

TCS CABLE Driver: https://schneider-electric.box.com/TCS-Cable-Driver
You may also need;
Modbus Driver 32bit; https://schneider-electric.box.com/Modbus-Driver
Modbus Driver 64bit; https://schneider-electric.box.com/Modbus-64bit

Schneider Electric United Arab Emirates