Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
Why do I get an error when I try to connect to ILS1R851S1390 with Lexium CT?
Lexium CT requires an additional motor database file in order to connect to ILS1R851S1390.

The motor database file is attached to this knowledge article

The file should be downloaded and then copied into the installation directory for the database files of Lexium CT.

For Windows 7 the location will be…   Program Files (X86)/Schneider Electric/Lexium CT/commontools/database

For Windows XP the location will be …. Program Files/Schneider Electric/Lexium CT/commontools/database

Customers using virtual machine installations must locate the “database” folder for their particular installation layout and paste the database file into the database folder.


rev 3-19-18


Schneider Electric United Arab Emirates

Attachment(s)
ids085300_01002.gdb [21.92 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: