Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 30 - Local annunciation?
LED indication on the Sepam front panel
- 2 LEDs indicate the unit operating status:
  • green LED ON: Sepam on
  • red “key” LED: Sepam unavailable (initialization phase or detection of an internal failure)
- 9 yellow LEDs:
  • pre-assigned and identified by standard removable labels
  • the SFT2841 software tool may be used to assign LEDs and personalize labels.
Local annunciation on Sepam’s advanced UMI
Events and alarms may be indicated locally on Sepam’s advanced UMI by:
- messages on the display unit, available in 2 languages:
  • english, factory-set messages, not modifiable
  • local language, according to the version delivered (the language version is chosen when Sepam is set up)
- the lighting up of one of the 9 yellow LEDs, according to the LED assignment, which is set using SFT2841.

Schneider Electric United Arab Emirates