What is the function of ACE850TP and ACE850FO network interfaces?
ACE850 multi-protocol communication interfaces are for Sepam series 40 and Sepam series 80 units.
They have two Ethernet communication ports to connect a Sepam unit to a sing
Ethernet network depending on the topology (star or ring):
1- IEC 61850
2- eModbus TCP/IP TRA 15.
They have two Ethernet communication ports to connect a Sepam unit to a sing
Ethernet network depending on the topology (star or ring):
- For a star topology, only one communication port is used.
- For a ring topology, both Ethernet communication ports are used to provide redundancy. This redundancy conforms to the RSTP 802.1d 2004 standard.
- To the S-LAN (Supervisory Local Area Network) port to connect a Sepam unit to
1- IEC 61850
2- eModbus TCP/IP TRA 15.
- To the E-LAN (Engineering Local Area Network) port, reserved for remote parameter setting and operation of a Sepam unit using SFT2841 software.
- ACE850TP (Twisted Pair), for connection to an Ethernet network (S-LAN or
- ACE850FO (Fiber Optic), for connection to an Ethernet network (S-LAN or E-LAN)
Released for: Schneider Electric United Arab Emirates