Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
What is the function of ACE917 injection adapter?
The ACE917 adapter is used to test the protection chain with a standard injection box, when Sepam is connected to LPCT sensors.

The ACE917 adapter is inserted between:
  • The standard injection box
  • The LPCT test plug:
- integrated in the Sepam CCA670/CCA671 interface connector
- or transferred by means of the CCA613 accessory.

The following are supplied with the ACE917 injection adapter:
  • Power supply cord
  • 3-meter (9.84 ft) cord to connect the ACE917 to the LPCT test plug on CCA670/CCA671 or CCA613.
Characteristics

Power supply: 115/230 V AC
Protection by time-delayed fuse 5 mm x 20 mm (0.2 x 0.79 in ):  0.25 A rating

Schneider Electric United Arab Emirates