Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
Easergy Micom P142 relay rebooted itself and came to normal healthy position. Why it has happened ?

Issue:

Reason for Easergy Micom P142 relay rebooted itself and came to normal healthy position

Product family:

Easergy Micom P142


Resolution:

As per the manual, the relay performs continuous self-checking, if an error is detected then an error
message will be displayed, a maintenance record will be logged and the relay will reset
(after a 1.6 second delay).
If the problem was transient in nature then the relay should reboot correctly and continue in operation.

A permanent problem (for example due to a hardware fault) will generally be detected on the power up sequence, following which the relay will display an error code and halt.
If you need any support, please contact with the below details to our customer care center :

1) .studiofile with setting,psl,mcl/ICD,logs(events,DR) extracted from relay (all the files in one system studio file)

2) Lable picture from front panel of the relay.

Schneider Electric United Arab Emirates