Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
How to implement DC braking in the ATV630?
DC injection braking is activated through below parameters

- Stt [Type of stop] = [DC injection] (dCI): DC injection stop ---> when you apply stop command the DC injection braking is active.
Or
- dCI [DC injection assign.] = LI1 to LIx ---> The DC Breaking is activated when you give this assigned Logic input LIx - When you apply this logic input (if assigned) it will apply DC injection breaking.

In addition to the following:
- IdC [DC inject. level 1] = 0.7 In (range 0.1...1.41 In)
- tdI [DC injection time 1] = 0.5 s (range 0.1...30 s)

Schneider Electric United Arab Emirates