Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
How to reduce starting current in ATS22?
Starting current is set into soft starter based on type of application and load demand.
Current can be limited from ILt from 200 : 700 % In (Motor rated current) and default value is 350%.
Also,decreasing ACC (Acceleration time) to shorten the period of starting.

Note:

Proper fine-tuning of the starting current (ILt) setting has to be done during commissioning.
Normally the soft starter will work without any problem with current limit setting between 200% to 450% for different application starting torque requirement.
For example : for compressor application starting current received is approx. 3 to 4 times the rated motor current.

Schneider Electric United Arab Emirates