How can we help you today?

What is the difference between P/N CCT15482 and P/N 15482? And are they compatible with analogue light sensor P/N CCT15263?

P/N CCT15482 is the new Acti9 IC100 twilight switch while P/N 15482 is the old platform IC100 twilight switch.

Old Platform P/N 15284 was delivered with a wall-mounted cell P/N 15268. P/N 15268 was never sold separately but only in combination with old platform IC100. If this cell got damaged, customer can order the spare wall-mounted cell P/N CCT15268.

New Platform P/N CCT15482 is delivered with a wall-mounted cell P/N CCT15268. P/N CCT15268 can be sold separately as a spare part.

According to the instruction sheet for Acti9 IC100 twilight switch P/N CCT15482, it is compatible with P/N CCT15263
https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=CCT15482_HW_all.pdf

However, the old platform of IC100 twilight switch P/N 15482 is not compatible with the new analogue light sensor P/N CCT15263.

Schneider Electric United Arab Emirates

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: