Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
How to configure Modbus setting in SE8000 series room controllers?

The SE8000 Series Room Controller acts as a Modbus slave by using its RS485 port. As BACnet and Modbus use the same RS485 port, a setup menu allows switching between the two protocols.
Setup modbus communication parameters
The full register list can be found at Modbus Integration guides that can be downloaded from Exchange for SE8300, SE8600, SER8300 and SEZ8250.

Schneider Electric United Arab Emirates