Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
How to connect Advanced display v3 (AD v3) to EcoStruxure BMS Server?

AD v3 can use either a wired (USB) connection or a wireless (WiFi) connection to communicate with EcoStruxure BMS

• USB Connection
AD v3 uses a wired (USB) connection to communicate with SmartX servers (AS/AS-P/AS-B) and the device must be powered by a 24 VDC power supply.  AD v3 must be powered by a 24 VDC power supply. The Y-shaped cable, ordered separately (SXWADUSBC10002 or SXWADUSBC10003) enables data communication and power supply over a single cable. Only cables designed for AD v3 must be used. The required cables can be ordered from Schneider Electric.
AD V3 Wired connection

Wireless connection:
AD v3 connects to EcoStruxure BMS Server (ES/AS/AS-P/AS-B) via Wi-Fi. Wi-Fi module needs to be ordered separately.
AD V3 Wireless connection
Commercial References:
AD V3 commercial reference

Schneider Electric United Arab Emirates