Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
SP-C controller doesn't reply to ping request
Issue:
SP-C controller is online but doesn't reply to ping request.

Environment:
EcoStruxure Security Expert, SP-C

Resolution:
As a Cybersecurity enhancement, ping is disabled by default for the onboard Ethernet connection on SP-C with firmware V2.08.825 or higher. It can be re-enabled via Controller Commands. You can also check SP-C online status on the Security Expert software or via the SP-C web interface.

Schneider Electric United Arab Emirates