How can we help you today?

Where can I get pre and post-transfer signals on series 300 with Group G controller?

To have pre and post-transfer signals available, feature 31 needs to be enabled.

For Series 300, a set of form C contacts are provided on the group G controller as "OP1".



When the feature setting of "OP1" is set to operate the contacts as "Feature 31", the time delay settings of the pre and post-transfer signals are available.



For further information, refer to page 11 of the Group G controller user's guide.  If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com

Schneider Electric United Arab Emirates