How to select the LPCT/LPVT option (offline) in Easergy P3 through Easergy pro software?
!!!Confidential Content
Description/Issue :
Select the LPCT/LPVT option (offline) in Easergy P3 through Easergy pro software?
Environment/Product line:
Easergy P3 relays
Resolution :
Please follow this procedure in case you need create off-line settings to Easergy P3 with LPCT options.
1. In the option 'X5' - Voltage Measurements + I/O option, should be selected the option 'C - 6DI + 3DO 2. After, Easergy Pro will be enabled the LPCT option on 'X1' - Phase Currents and voltage input as '7/8-for 3xLPCT+5xLPVT
After the above configure the device will support for LPCT/LPVT
Released for: Schneider Electric United Arab Emirates