How can we help you today?

Can we use Easergy Micom Px4x relays selected with PRP for single network communication?

Description:
Possibility to use Easergy Micom Px4x relays with PRP for single network communication

Environment/Product line:
Easergy Micom relay

Resolution:
Please select the dual IP after that it is possible to select one network as require.

Kindly do not hesitate to refer to manual to set your device in accordance with your network topology.


Schneider Electric United Arab Emirates

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: