In VAMP 321, What is the next step to be done after physically connecting the arc sensors and the I/O units to the relay?
Issue,
Customer want to know what is the next step to be done after connecting the sensors to the I/O unit
Resolution:
VAMP 321
Environment:
After physically connecting the sensors and the I/O units to VAMP 321 relay, the following steps must be done. These steps are to be done at the beginning of the project installation and repeated after adding or removing any sensor or I/O unit at any time.
1- Make sure you are connected to the relay
2- In VAMPset, Go to Arc protection menu
3- Go to "Install arc sensors & I/O units " menu and select install.
4- "Installation state' is then changed from ready to installing
5- when installation is finished, the installation state will go back to ready.
Released for: Schneider Electric United Arab Emirates
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.