In applications where there is prolonged exposure to direct sunlight (UV), the use of double-door Secure UL Type 3R enclosures (code ‘M’ in the catalog string) is recommended so that the controller and meter front faces are protected by the outer door. If a standard, non-secure UL Type 3R (enclosure code ‘F’) was ordered, cover kits can be purchased and field-installed to provide protection in the absence of the outer door.
The orderable kit numbers are the following:
K1200209-001
ATS METAL DOOR COVER KIT FOR
GROUP 5 OR GROUP G IN NON-
SECURE 3R ENCLOSURE
Includes:
- hasp
- protective door cover
- Installation instructions
K1200209
ATS METAL DOOR COVER KIT FOR
5210 OR 5220 METER IN NON-
SECURE 3R ENCLOSURE
Includes:
- hasp
- protective door cover
- Installation instructions
To order the cover kits, please reach out to ASCO Parts at parts@ascopower.com or dial 1.800.800.ASCO (2726) and follow the voice prompt to select the Parts Department.
To request a digital copy of the related Installation Manual 381339-330, please reach out to technicalsupport@ascopower.com or dial 1.800.800.ASCO (2726) and follow the voice prompt to select Technical Support.
Released for: Schneider Electric United Arab Emirates