Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
		
How can we help you today?
Can two or more ASCO transfer switches be connected to and able to start a common generator?
YES, two or more ASCO transfer switches can be connected to a common generator and any transfer switch can start the generator.

The generator start wires must be connected to the “engine start contacts” of one of the transfer switches.  Then, the “engine start contacts” of each transfer switches must be connected in PARALLEL.

In this configuration, using the sample diagrams below, any of the transfer switches that loses its primary power, and closes its start contacts in the process, will send a start signal to the generator.

Engine Start Wires Parallel Connection

Genset Start Wires Parallel Connection

Schneider Electric United Arab Emirates

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre