How can we help you today?

How to save the communication and operation report of an explicit communication like Read_Var EF using an ST section

In the Control Expert documentation, you can see the below :
doc CE
See below an example of an ST section that will record the communication and operation report value of an explicit communication EF (So the Management_Table[1] of this EF) and will check and reset accordingly the function management parameters  :

st

This ST section is also available in attachment

Schneider Electric United Arab Emirates

Attachment(s)
( Read_Var ETH ).txt [888 Bytes]
St section.zip [974 Bytes]