How can we help you today?

What is the cause of the FWPF error on an ATS480?

Issue:

What are the possible causes of an FWPF error on an ATS480?

Product Line:

ATS480

Environment:

Display shown on the VW3A1111 keypad

Resolution:

If the ATS480 is powered on with the VW3A1111 keypad and it displays a FWPF fault, with the soft starter powered off, remove the VW3A1111 keypad and connect the mini keypad that comes with the unit. Then power it back on and press OK to clear the fault.

Schneider Electric United Arab Emirates