What baud rates are supported by the EM4200 Series Power Meter?
Issue
Customer is looking for device communication specifications and needs to know the baud rates that are supported by the device.
Product Line
EM4200 Series Enercept Power and Energy Meters
Environment
Hardware & Hardware Communications (Modbus, BACnet, etc.)
Cause
The supported serial communication rates and automatic communication detection capabilities need clarification.
Resolution
Communicating models of the EM4200 Series automatically detect the baud rate, parity, and communication protocol.
The meter supports Modbus RTU and BACnet MS/TP communication at serial rates up to 115.2 kbaud, equivalent to 115,200 baud.
Additionally, The EM4200 also automatically detects and selects the appropriate communication protocol and parity settings.