Technical FAQs

Ask a Question

Filter results

Clear
Which communication protocol is used between a Compact NSX and display FDM121.
The communication protocol used between the Compact NSX and FDM121 display is Universal Logic Plug (ULP). This a Schneider Electric internal protocol.
What is the Modbus TCP/ IP option for a ATV660 ?
Issue:  What is the Modbus TCP/ IP option for a ATV660 ? Product Line: ALTIVAR PROCESS SYSTEM Environment: All   Cause: Product Selection & Services...
What are the part number and driver for the serial port (9-Pin D-Shell) to USB converter for Modicon Quantum PLC.
The part no. of the Schneider USB to RS232 Converter is TSXCUSB232 Refer the attachment for the TSXUSB232 documentation.   Use the standard Schneider...
What communication options (network protocols) are supported by the ATV312?
Issue:  What are the communication protocol that are available on the ATV312? Product line:   Altivar 312 Environment:   All range  All serial number   ...
What do the LED's indicate on the ATV58 Devicenet card?
Issue: What do the LED's indicate on the ATV58 Devicenet card?   Product Line: ATV58   Environment: All models and serial numbers with VW3A58309U...
What is the broadcast address in terms of Ethernet network.
A broadcast address is an IP address that is used to target all systems on a specific subnet network instead of single hosts.   In other words broadcast...
What is the difference between ModSoft PID function and Concept PID function.
The difference between ModSoft PID and Concept PID loops are as follows:  PID (ModSoft):                                                                  ...
Which Modbus functions are used for reading/writing multiple data on IO scanning in Modicon Quantum range.
In Modicon Quantum range, I/O scanning works with following Modbus function codes:   FC3 for Reading Multiple 4X registers. FC16 for Writing Multiple...
How to convert DINT variable to REAL variable in Concept (with IEC disabled).
In order to convert DINT variable to REAL variable in Concept (with IEC disabled) make use of EMTH-CNVIF instruction.
How to calculate the scan time of Hot Stand-By (HSBY) system in Modicon Quantum range.
Considering the Hot Stand-By system, the scan time mainly comes from the addition of three parts:   Part 1: User application logic execution time,...
Results 1 - 10 of 39