{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.

What is the definition of ANSI 46 - Negative sequence / unbalance?

Protection against phase unbalance, detected by the measurement of negative sequence current: sensitive protection to detect 2-phase faults at the ends of long lines protection of equipment against...

What is the calculation for heat dissipation in BTU/HR?

Issue: How to calculate the heat dissipation in BTU per hour Product Line: All Schneider product lines Cause: The calculation to determine the BTU for adding a piece of equipment to a cabinet to...

What is the definition of ANSI 50N/51N or 50G/51G - Earth fault?

Earth fault protection based on measured or calculated residual current values: ANSI 50N/51N: residual current calculated or measured by 3 phase current sensors ANSI 50G/51G: residual current...

What is the definition of ANSI 50BF - Breaker failure?

If a breaker fails to be triggered by a tripping order, as detected by the non-extinction of the fault current, this backup protection sends a tripping order to the upstream or adjacent breakers.

What is the definition of ANSI 67N/67NC - Directional earth fault?

Earth fault protection, with selective tripping according to fault current direction. 3 types of operation: type 1: the protection function uses the projection of the I0 vector type 2: the protection...

What is the Utilisation cat for NS MCCB and ICS and ICU percentage ?

IEC 60947 define ICS as the "rated service short-circuit breaking capacity" while ICU as the "rated ultimate short-circuit breaking capacity". The Ics is a percentage of Icu. For...

What is the Restricted earth fault protection and how to implement on Low...

The restricted earth fault protection (ANSI 64REF) can be applied if the downstream power system neutral is earthed at the transformer (document attached). This is a differential protection function...

What are the main differences between between IEC rated breakers and UL...

Although almost 80-90% of the features are the same, there are differences between the IEC and UL(NEMA)/ANSI/CSA breakers. Depending on the frame, the following components may be different: •...

Show more

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
Show more

Learn more through our Generic Knowledge FAQsGeneral Knowledge

What is meant by Symmetrical and Asymmetrical breaking currents?

issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...

Apa alternatif replacement battery UPS SURT15KRMXLI jika APCRBC140 tidak...

Apa alternatif replacement battery UPS SURT15KRMXLI jika APCRBC140 tidak ready stock? ======================================================================= Untuk alternatifnya bisa menggunakan...

In a 3 phase system, why does the meter still show voltage reading on one...

Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...

How to reset Zelio logic password?

The password can be reset by clearing the program inside the Zelio either by Transfering a new program to the Zelio Or Clearing the program that already exist by updating the firmware Kindly find the...

What is the selection criterion of Circuit Breakers for the Capacitor bank...

The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase nominal current up to 1.5In. The Derating...

Show more