Do you have a library with the electrical symbols of the devices, specifically for the Acti9 iC60N series in DXF format ?
We do not have a library with the electrical symbols of the devices.
These symbols are not specific to a manufacturer.
The iC60N is a circuit breaker with thermal and magnetic protection (overload and short circuit protection). The standard MCB symbol can be used to represent it in a schematic.
These symbols usually are either created by the CAD user or possibly downloaded from a library that is available in the CAD drawing software used.
For example, Autocad Electrical has a library for such electrical symbols.
Released for: Schneider Electric Belgium
Need help?
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.