The VigiPacT RHB relay is compatible with ComPact NSX/NSXm; it is not designed to be used with iC60, C120, or NG125.
The VigiPacT RHB relay is compatible with the following circuit breakers:
• ComPacT NSX 100-250
• ComPacT NSX 400-630
• ComPacT NSXm 16-160
The VigiPacT RHB relay is compliant with the standard IEC/EN 60947-2 annex M.
See page 7 in the User Guide. See the link to this document:
https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=DOCA0160EN-00.pdf&p_Doc_Ref=DOCA0160EN