Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to combine two PrismaSeT XS or S enclosures without using kits, and if so, what is required for this setup?

Article available in these languages: French, Dutch

A combination of 2 PrismaSeT XS or S enclosures is only possible with a cut-out in the side. The range does not include kits to attach 2 enclosures together. 2 side by side, or 1 above and 1 below, each with the same dimensions. These are therefore not designed to attach the enclosures together. When you look at the PrismaSeT G range, there are also enclosures for wall mounting. And there are kits available to place them side by side or on top of each other.

Schneider Electric Belgium

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Substitution and Replacement
  • Help and Contact Center