How can we help you today?

Concerns reference LV432641 - How do I mount the motor for a Compact NSX400-630N/H/S/L ?

We can use the 'Instruction Sheet' for this. See the link:


https://download.schneider-electric.com/files?p_enDocType=Instruction+sheet&p_File_Name=Motor-Mechanism-Instruction-Sheet-BQT6157605-00.pdf&p_Doc_Ref=BQT6157605


  • To simplify things, we will start by assembling only the motor. Then, we will perform a test in 'Manual' mode.


  • Only afterwards will the MN coil be installed. To be able to test the motor with the MN coil, the MN coil must be powered. Then, we will perform a test in 'Manual' mode with the motor.


In addition, I can share a video showing the installation of a motor on a Compact NSX. See link:


https://www.youtube.com/watch?v=9NnEB6bcGjQ



The warning included in the motor's packaging concerns the fact that the inside of the motor should not be handled, in order to avoid altering or damaging the position of the internal components.

​​​​​​​



Schneider Electric Belgium