Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is ComPacT NSX100-250 UL508A Listed or Certified ?

Article available in these languages: French, Dutch

A transition has been made in the standard from UL508 to UL 60947-4-1, in order to harmonize with the IEC standard.

ComPacT NSX complies with this UL 60947-4-1 standard for performance levels F, N, and H. So not for B.

Therefore, you should select for example C10F4 to be compliant.

This is also indicated on pages A-6 and A-7 of the catalog. In the Belgian Dutch-language and French-language catalog, you will still find UL508, while the English-language catalog mentions UL 60947-4-1.

Schneider Electric Belgium

Attachment(s)
UL Certificate NSX ComPacT 100-250.pdf [148.58 KB]
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: