UPS battery backup for retail POS and kiosks
UPS with SmartConnect
UPS battery backup for retail POS and kiosksPower every point of sale (POS), kiosk, and customer experience with integrated IT infrastructure solutions that put you in control.

Your IT must keep up
Retail runs on constant connectivityIntelligent power protection by EcoStruxure™ IT SmartConnect safeguards operations keeping your point of sale POS, self-serve kiosks, ATMs and critical systems running for seamless customer experiences.
Powering always-on retail experiences
Protect every transaction to deliver the connected retail experience your customers expect.
Powering always-on retail experiences
Protect every transaction to deliver the connected retail experience your customers expect.

Hardware meets software
Smarter togetherTransform our trusted Back-UPS systems into intelligent, connected assets that support retail IT applications across every location, providing real-time visibility with EcoStruxure IT SmartConnect.

Simplify retail IT operations with EcoStruxure IT SmartConnect cloud monitoring - securely and seamlessly
Insights from anywhere
Cloud monitoring via PowerChute link
Eliminate estimation
Events logs and uptime summary reports
Improve availability
Proactive device health and status
Actionable insights
Battery insight and lifecycle tracking
Remote power monitoring
Monitor sites that lack IT expertise
Centralized visibility
Easily view devices in map or table view
Service savings
eMail alerts to detect issues early
Select the UPS and SmartConnect solution that’s right for your needs.
BE Series | BK Series | BR Series | |
| Action | |||
| UPS Series | |||
| Power rating (VA) | 650 - 850 VA | 350 - 650 VA | 650 - 900 VA |
| Power ration (Watts) | 400 - 520 Watts | 210 - 400 Watts | 400 - 540 Watts |
| Runtime based on 119W | 20 - 28 mins | 20.5 - 26.5 mins | 26.5 - 30 mins |
| Automatic Voltage Regulation (AVR) | No | Yes | Yes |
| Number of outlets | 8 outlets | 6 outlets | 6 outlets |
| User replaceable battery | Yes | Yes | Yes |
| Dimensions (HxWxD) | 120 x 130 x 365 mm | 190 x 91 x 310 mm | 190 x 91 x 310 mm |
| Remote management (via PowerChute link to SmartConnect cloud) | Yes | Yes | Yes |
Increase efficiency and performance by connecting your Back-UPS to EcoStruxure IT SmartConnect
Speed to scale
I blocked off two days to deploy the solution, but it only took five minutes.
Access from anywhere, any time
I needed a way to quickly check the status of all my data closets at any time from any location. Now I simply look at my phone for easy access.
Full visibility
I'm kept up to speed on issues with my UPS and resolutions so that I can prioritize my workload.
Lack of on-site IT support
It allows retail associates to spend more time connecting with customers and less time managing systems.
Reduced labor costs
Getting ahead of a potential problem can give back 3,600 staff hours across sites.
Small footprint
Retail space is limited and managing this emerges as a critical success factor.
Retailers need robust, secure, multi-site IT management platforms with remote capabilities to ensure all their locations stay trouble-free, resilient, and secure.

Need help?
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.
What UPS is best for a retail point of sale (POS), kiosk, or terminal?
For retail POS systems, kiosks, and payment terminals, an APC Back-UPS is often the best choice because it provides reliable battery backup, power protection, andremote monitoring. With SmartConnect models that support remote management, retailers can proactively monitor UPS status, receive alerts, and reduce downtimeacross single or multi-site locations—helping keep transactions running smoothly during power disturbances.
Can you manage a UPS in a retail point of sale (POS), kiosk or terminal location?
Yes. APC™ UPS solutions with remote monitoring capabilities allow IT teams to monitor, manage, and receive alerts from UPS devices across POS terminals, kiosks,and retail locations from a centralized dashboard. This helps improve uptime, simplify maintenance, and proactively address power issues before they impact customertransactions.
What provides additional runtime for retail point of sale (POS), kiosk, or terminal?
Additional runtime for retail POS systems, kiosks, and terminals can be achieved by using an APC Back-UPS™ sized for the connected load and desired runtime. Thesesolutions help keep critical retail operations running longer during power outages, maintaining uptime for critical operations, ensuring systems safely completetransactions and recover cleanly.
What is UPS in retail?
In retail, a UPS (Uninterruptible Power Supply) is a battery backup device that provides temporary power and protection for critical equipment such as POS systems,kiosks, payment terminals, and network devices during power outages or disturbances. APC™ UPS solutions with remote monitoring capabilities help retailers maintainbusiness continuity, reduce downtime, and proactively manage power infrastructure across one or multiple store locations.
What is a point of sale (POS) kiosk UPS?
A POS kiosk UPS (Uninterruptible Power Supply) is a battery backup system designed to protect point-of-sale terminals, self-service kiosks, and payment devices frompower outages, surges, and voltage fluctuations. APC™ UPS solutions help keep transactions running during power disruptions and, with SmartConnect remotemonitoring capabilities, enable IT teams to proactively manage and monitor power protection across retail locations.
What is the risk of a point of sale (POS) experiencing downtime?
There are many costs when it comes to downtime in a retail space - not just lost revenue. There are lost transactions, abandoned carts, damaged customer experience, lost productivity, inventory drift. Here are some industry statistics to put it in perspective:
Studies found 67% of customers who experience payment issues during a store visit don’t return to complete the purchase later.
The true cost of POS downtime and how to prevent it
According to the annual outage analysis of 2025 by the Uptime Institute the most common cause of downtime is power outages and fluctuations at 54% of incidents.
“The Cost of Downtime: Beyond the Bottom Line,” a study released by Cronus Communications shows that 20 percent of retailers respondened that they do not have backup connectivity solutions in place. While 72 percent of retailers surveyed indicated sales were lost during network downtime.
Study finds vast majority of retailers still vulnerable to network downtime
Statistics show that 81% of retailers experience POS downtime at least once a year, and 87% of those businesses wait four hours or more for support from their POS supplier. Here are the figures that really make you sit up and take notice. 98% of organizations say a single hour of system downtime costs their business over $100,000. 81% say it costs them more than $300,000.




_BUILDER.IORectangle.webp)